busway

Busway Gives You Flexibility and Scalability

đź•“ 3 minute read

It is not the strongest of the species that survives, nor the most intelligent that survives. It is the one that is most adaptable to change. – Charles Darwin

In today’s dynamic and unpredictable world, the companies that will thrive are not necessarily the largest or most innovative but have the flexibility to adapt quickly to changing needs and unexpected events. These companies also seek power that is on demand with no downtime. A reliable power distribution system is essential for any data center, manufacturing plant, or industrial facility. Unfortunately, traditional pipe & wire systems don’t have the flexibility to handle quick changes in layout and machinery on the factory floor. Traditional power distribution methods can involve high labor costs, complicated scheduling, and potentially considerable downtime.

Track Busway

An effective and reliable power distribution system is essential. For decades, companies relied on traditional electrical conduit and wiring systems —informally known as “pipe & wire systems”— to deliver power.

But traditional pipe & wire systems have numerous drawbacks, including installation time and their lack of flexibility in adapting to changes.

Fortunately, there is an alternative.

Overhead power distribution using track busway systems is rapidly becoming the solution of choice in data centers, industrial and manufacturing plants, and other facilities that require continuous uptime and faster adaptability.

Track busway systems offer numerous advantages over traditional power systems. Suspended or mounted track busways eliminate the need for a remote power panel (RPP) in data centers or pipe and wire electrical distribution in these other facilities, providing flexibility and scalability for electrical reconfiguration.

Our busway systems can be installed up to 90% faster than traditional pipe & wire systems, with far less installation labor.

A track busway system provides the same high-performance power delivery as traditional pipe & wire systems. But track busway also offers the flexibility to make quick and easy changes in your power distribution layout and the scalability to accommodate additional and/or higher power loads. A track busway system lets you adapt your power distribution to the changing needs of your facility with less trouble and cost.

Unlike traditional wiring, open channel busways enable operators to relocate power access points/outlets directly where power is needed in a matter of minutes without contracting ever-scarce electricians.

With traditional busway systems, companies must do regular maintenance, which necessitates shutting down power. However, Starline Track Busway is a maintenance-free system where you do not need to shut down the power. There’s no downtime, so using it enhances the facility’s reliability. Starline track busway provides a competitive advantage, allowing facilities to stay operational—ensuring companies will always be productive and able to deliver products or services to their customers.

Finally, Starline busway helps companies achieve sustainability goals because all system components can be disassembled and reused at new locations.

For installations, large or small, there is a solution that makes sense in Starline’s leading portfolio of products. To learn more about how track busway can bring flexibility to your facility, visit starlinepower.com/busway/ 

Tags
Track Busway
  • Join Our Mailing List